Cookies auf der SKF Webseite

Wir von SKF verwenden Cookies auf unserer Website, um die angezeigten Informationen optimal auf die Interessen der Besucher abzustimmen, wie z. B. auf die bevorzugte Länder- oder Sprachwahl.

cookie_information_popup_text_2[49]

SKF Bearing Select

Please, use the new version of SKF Bearing Select*. It has a fully updated, clean and user-friendly interface. Calculation results can be obtained faster and are presented directly near the required input data. This new version has been designed in alignment with the new Bearing Selection Process. In addition, more bearing performance results are calculated:

  • Bearing friction and power loss
  • Adjusted reference speed
  • Minimum required load
  • Grease life for capped bearings
This new version of SKF Bearing Select is under development, therefore not all functionalities are finalized. For the following calculations, please use the previous version of SKF Bearing Select:
  • Two bearings on a shaft
  • Load cycle analysis
  • Static safety
SKF logo