Cookies auf der SKF Webseite

Wir von SKF verwenden Cookies auf unserer Website, um die angezeigten Informationen optimal auf die Interessen der Besucher abzustimmen, wie z. B. auf die bevorzugte Länder- oder Sprachwahl.

cookie_information_popup_text_2[49]

Ordering information

For SNL and SE plummer (pillow) block housings in the 2, 3, 5 and 6 series, each of the following items must be ordered separately:
  • housing
  • seals
  • end cover
  • locating rings
  • bearing
  • adapter sleeve

Order example

Two plummer block housings with four-lip seals are required for two 22218 EK spherical roller bearings on H 318 adapter sleeves. One housing will accommodate the non-locating bearing at the end of the shaft. The other housing will accommodate the locating bearing and a through shaft.
The following items should be ordered (in addition to the bearings and adapter sleeves):
  • 2 housings SNL 518-615
  • 2 four-lip seal packs TSN 518 L (each pack contains two seals)
  • 1 end cover ASNH 518-615
  • 2 locating rings FRB 12.5/160
SKF logo